Browse FAQs

IONMaintenance user does not have "Log on as a batch job" rights

Published date: 17 June 2020

Issue
The Windows Scheduled Tasks for the Database Maintenance jobs fail to run. The jobs fail with an error stating that the IONMaintenance account does not have "Log on as a batch job" rights


Product Line
Power Monitoring Expert 8.x

Environment
Windows Task Scheduler 

Resolution
Follow the steps described below  to give IONMaintenance user Log on as a batch job rights. This will allow the IONMaintenance user to run tasks in the Task Scheduler when the user is not logged on.

  1. Go to the Start menu
  2. Run
  3. Type secpol.msc and press Enter
  4. The Local Security Policy manager opens
  5. Navigate to Security Settings -> Local Policies -> User Rights Assignment 
  6. Double click Log on as a batch job on the right side
  7. Click Add User or Group...
  8. add IONMaintenance user and make sure to click on Check Names, then click OK.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.