Browse FAQs

What list of parameters can be read over Modbus/BACnet protocols on the ATV212 drive?

Published date: 15 June 2020

Issue:
List of parameters that can be read over Modbus/BACnet protocols on the ATV212 drive

Product Line:
Altivar 212

Environment:
All

Cause:
Communications

Resolution:

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.