Browse FAQs

"Out of licenses for IE7_server" error in FlexNet Publisher

Published date: 19 June 2020

Issue
A user is seeing the following error message in the Flexnet Publisher client.
"Out of licenses for IE7_server"

Product Line
Power Monitoring Expert 8.0

Environment
Software licensing 

Cause
This can happen if the ION Site service stops or crashes unexpectedly. When this occurs, the vendor daemon will think the IE7_server feature is still signed out. Therefore, when the ION Site service requests for the feature again, the license request will fail.

Resolution
Restarting the lmadminSchneider service should release the feature license and correct the condition.
Note: If the issue continues in the future, further troubleshooting will be required to see why the ION Site service may be crashing.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.