Browse FAQs

How do you set up the ATV630 drive to work with a M340 PLC to read modbus registers only over Ethernet without IO scanning?

Published date: 12 June 2020

Issue:
ATV630 set up for working with a M340 PLC to read modbus registers only over Ethernet without IO scanning.

Product Line:
ATV630 with M340 PLC

Environment:
All 

Cause:
Wants to read 4X registers over Ethernet on the ATV630 drive. 

Resolution:
You will need to set up the Drives modbus address to 1 (power cycle the drive after you set the modbus address.   The PLC will also need to be set up for Unit ID 1.
Example setting up the M340 go to the ADDM block and add the unit ID number 1 behind the last curly block.  Before Example  {123. 345.345}  After Example  {123. 345.345}1
Now you can read and write var modbus address to and from the drive thru the master or PLC.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.