Browse FAQs

How do you wire in the RL line reactor when using single-phase input three-phase output on a ATV71 drive?

Published date: 29 June 2020

Issue:
RL line reactor wiring when using single-phase input three-phase output on a ATV71 drive

Product Line:
ATV71 and ATV61 1 phase input only

Environment:
All 

Cause:
Wiring up RL line reactor with 3 inputs when drive is single phase input. 

Resolution:
You will wire L1 to 1st outside terminal on the RL line reactor. 
You will wire LI2 on the 3rd outside terminal on the RL line reactor. 
Leave the middle connection on the RL line reactor blank.
Reference 30072-451-38

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.