Browse FAQs

Can the firmware of the ATV340 be updated in the field?

Published date: 19 June 2020

Issue:
ATV340 firmware update

Product Line:
Altivar 340 series drives.

Environment:
All models, All serial numbers.

Cause:
Information unavailable in current literature.

Resolution:
Currently, the ATV340 series drives will need to be returned to Schneider Services if the firmware needs to be updated. In the future, it may be possible to update the firmware in the field. Note that, all new purchases from Schneider Electric will have the latest version of firmware installed from the factory.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.