Browse FAQs

What are the new features in SoMachine Basic v1.5 SP1?

Published date: 29 June 2020


This SoMachine Basic v1.5 SP1 Service Pack addresses the following security strategy modifications:
  • Reinforce Application Protection (requires an upgrade to the latest Functional Level and Firmware)
  • Reinforce the project file encryption when enabling the Project Protection
  • The "download only" mode is no longer available from the Project Protection view.
    "Restore to Controller" feature is available for this purpose. It requires the smbk file generated by the "Create Controller image" feature (available within the Memory Management view)
  • The communication with some ION meters has been improved

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.