Browse FAQs

What is the replacement for Berger Lahr part number MNA3MF10/5/12 ?

Published date: 04 September 2019

The part number of MNA3MF10/5/12 is for "clamping claws" used to mount PAS42 linear acuators.

These clamping claws are available in various sizes depending on which axis is being used.
The specific model of MNA3MF10/5/12 is for use with PAS42 type axis and the part number has been changed to VW33MF10512.

Attached to this knowledge article you will find the complete list of clamping claws based on the old part numbers and new part numbers.
Compare the two attached files and choose the correct part number needed from the "new" list.

rev 9-4-19




 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.