Browse FAQs

How can you setup Pipe Fill on an Altivar 61 without the water solutions or pump control card?

Published date: 29 June 2020

Issue:
Need to configure ATV61 for Pipe Fill with no option card

Product Line: 
Altivar 61

Environment: 
All

Cause:
AC Drive ratings

Resolution: 

ATV61/71 Parameter Set Switching (with Pipefill / no Water Sol Card)
LI1 in Hand = Ref 1 Channel  to  AI1
LI1, LI3 in Auto  Ref 2 Switching LI3, Ref 2 Ch AI1
PID Ref AI2 (already done PID and it's working)
LI1 or LI1, LI3 with LI5, L6 for Pipe Fill
for the PipeFill function 
LI5 is assigned to PI Auto/Manual, and 2 Parameter Sets
LI6 is assigned to Preset Speed to with SP2 at 43Hz
Parameter Selection is Acceleration
Parameter Set 1 Acceleration is 2s 
Parameter Set 2 Acceleration is 200s

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.