Browse FAQs

What can cause Err6 code on an ATS48 remote keypad?

Published date: 15 June 2020

Issue:
Err6 code on an ATS48 remote keypad

Product Line:
Altistart 48

Environment:
All

Cause:
Error, fault

Resolution:
This is an issue where the softstart is not communicating with the keypad.
This can be caused when utilizing a port expander to talk network while still using a remote keypad.
Normally you can only a keypad or network connection at a time.  With the expander you can achieve both.
Make sure that the network communications are set in the softstart.  Having an address of 0 will hinder the user from achieving connection.
Check main display of the softstart for possible issues.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.