Browse FAQs

What can cause an COF code or CANopen fault on the ATV312 drives?

Published date: 08 June 2020

Issue:
COF or CANopen fault on the ATV312 drives.

Product Line:
Altivar ATV312

Environment:
All 

Cause:
• Interruption in communication on the CANopen bus

Resolution:
Drives Programming check the CANopen Address and bit rate settings in the communications menu. 

Wiring:  Make sure you are using correct Purple CANopen cables and TAPs.   Follow the maximum wiring distances for any CANopen cable lengths.   See the attached document on wiring examples. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.