Browse FAQs

Why can't the motor current be read via Devicenet on ATV630?

Published date: 24 June 2020

Issue:
Cannot read the motor via Devicenet on ATV630

Product Line:
ATV630

Environment:
ATV630 communicating with Allen Bradley PLC

Cause:
Cannot read motor amps

Resolution:
On ATV630, the parameters for Devicenet scanner are not the same compared to ATV71.
ATV71 uses NCAx and NMAx
ATV630 is like ATV32/ATV320. It uses OCAx - OMAx
User-added image

To change the Monitoring parameter, configure it in SoMove.
User-added image

Today, it’s not possible to change these parameters via Graphic keypad Display (evolution request has been submitted).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.