Browse FAQs

How to observe the changes to graphic screens in Runtime without restarting the project?

Published date: 10 June 2020

Issue
Some graphic screens have either changed or new ones added. The updates should be seen in the HMI client, while the project remains running.

Product Line
PowerSCADA Expert (applies to PSO9.0 and older versions)

Environment
Runtime, Graphics Builder

Cause
Prevent the need to shutdown/restart of all processes.

Resolution
A. Modifying Existing Graphics Pages
1. After modifying a graphics page, save the page and re-compile the project.
2. In the HMI client, reload the page by navigating away from it and then returning to it.

B. New Graphics Pages
1. After adding new graphics pages, save the pages and re-compile the project.
2. Restart the HMI client only. It is not necessary to restart any other server processes.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.