Browse FAQs

What is the condition for Phase Loss Fault in EOCR-i3DM (Z, S, 420) / iFDM (Z, S, 420)

Published date: 25 June 2020

Phase loss fault comes into play in EOCR-i3DM (Z, S, 420) / iFDM (Z, S, 420) when max imbalance is more than 85% among 3 phase current.

Where,Imbalance factor (%) = (Imax phase - Imin_phase) / Imax_phase x 100%

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.