Browse FAQs

ION7650 series current input F measuring range and accuracy

Published date: 20 May 2020

Issue
Customer would like to know further details about the current option F for the ION7650.

Product Line
ION7650

Environment
Current Probe input for ION7650 series meter

Cause
What is the measurement range of the input to current option F.
What is the accuracy range of the input to current option F.

Resolution
For the ION7650 series current input F (Current Probe Inputs (for the 0-1 V AC current probes; sold separately)):
  1. The measurement range is 50mA to 100A
  2. The accuracy is 1% from 0.1 IN to 1.2 IN
Note: The current input F (current probe input) is not manufactured by Schneider Electric. The part number for this current input F is M1 UB 10A / 1V. For detailed information about the current probe input, please refer to the datasheet or visit http://www.universal-technica.com/en/www/pinces-micros.php for more information.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.