Browse FAQs

What is the difference between AC support Voltage(SW)/Grid Support Voltage(XW) and Recharge voltage?

Published date: 21 May 2020

Issue:
What is the difference between AC support Voltage(SW)/Grid Support Voltage(XW) and Recharge voltage?

Product Line:
Conext SW/XW+ System

Environment:
Parameter difference in Inverter Systems

Cause:
N/A

Resolution:
Recharge voltage is the setting/voltage level at which the inverter will start charging the batteries using AC input.

AC support Voltage(SW)/Grid Support Voltage(XW) is the Voltage level at which the Inverter will decide whether to stop (if lower) or start (if higher) supporting power to the loads.

Note:
If load Shave is enabled look at FA229629 for Load Shave explanation.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.