Browse FAQs

Screw replacement size for CL inverters and wiring box covers

Published date: 21 May 2020


Issue:
Screw replacement size for CL inverters and wiring box covers

Product Line:
CL Inverters

Environment:
Cover Screw replacement

Cause:
Lost Screws

Resolution:
Screw size is M5 x 15mm stainless machine screws and washers.
These can be found at any Rona, Lowes, Home Depot or Canadian Tire store, etc.

Note:
The CL25 should not be operated if its IP65 seal is compromised. Some components are prone to premature failure if exposed to moist, humid (aka Ontario) conditions so be careful.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.