Browse FAQs

What is the response time in the event of fault for the RM17 and RM35 Zelio control measurement relays?

Published date: 12 July 2018

Issue:
Fault response time for the Zelio RM17 and RM35 relays

Product Line:
Control and Measurement Relays

Environment:
Zelio Control Measurement Relays

Resolution:
RM17TG* - 100 ms maximum
RM17T•00* - <200 ms
RM35TF* - <200 ms
RM17UB3* - <200 ms
RM35UB3* - <200 ms
RM35BA* - <300 ms

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.