Browse FAQs

What are the part numbers for the EM4900 series meters?

Published date: 03 June 2020

Issue
What are the part numbers for the EM4900 series meters?

Product Line
EM4900 series meter

Environment
Part numbers

Cause
Part number options for the EM4900 series meter

Resolution

EM4900 Models:
Part Number Description
METSEEM4904A Multi-circuit meter - (4) 3-phase meters - Modbus RTU only
METSEEM4908A Multi-circuit meter - (8) 3-phase meters - Modbus RTU only
METSEEM4914A Multi-circuit meter - (14) 3-phase meters - Modbus RTU only
METSEEM4928A Multi-circuit meter - (28) 3-phase meters - Modbus RTU only
METSEEM4904E Multi-circuit meter - (4) 3-phase meters - Ethernet and serial (Modbus, BACnet, and SNMP)
METSEEM4908E Multi-circuit meter - (8) 3-phase meters - Ethernet and serial (Modbus, BACnet, and SNMP)
METSEEM4914E Multi-circuit meter - (14) 3-phase meters - Ethernet and serial (Modbus, BACnet, and SNMP)
METSEEM4928E Multi-circuit meter - (28) 3-phase meters - Ethernet and serial (Modbus, BACnet, and SNMP)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.