Browse FAQs

Can modbus data recorder retrieval be done on the PM8000 series meter?

Published date: 03 June 2020

Issue
Can modbus data recorder retrieval be done on the PM8000 series meter?

Product Line
PM8000 series meter

Environment
Modbus

Cause
Is it possible to retrieve the data records via modbus communications.

Resolution
The modbus read and writes of data recorders on the PM8000 series meter is not fully implemented. This feature was not tested, documented or released and as such will not function.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.