Browse FAQs

Why is the TMH2GDB not connecting to the M221?

Published date: 29 June 2020


Answer
Issue:
Getting an incompatible device error.

Product Line:
TMH2GDB V1.0
M221 

Resolution:
The firmware needs to be updated
If the value in %SW185 is 100hex, the unit must be exchanged as it is not possible to update the firmware in the field. 
If %SW185  = 0103 you can upgrade the firmware.  Follow the instruction in the TMH2GDDB user manual attached below
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.