Browse FAQs

What are the recommended ribbon cables for the BCPM printed circuit board?

Published date: 04 June 2020

Issue
What are the recommended ribbon cables for the BCPM printed circuit board?

Product Line
BCPM

Environment
Cabling and connection

Cause
How to select Flat ribbon cable vs Round ribbon cable.

Resolution
Flat ribbon cables are recommended for use when the BCPM printed circuit board will be mounted inside of the PDU that is being monitored. Round ribbon cables are the preferred choice when the ribbon cable will be threaded through conduit.
 
Commercial Reference Number Ribbon Cable for use with BCPM products
CBL016 Flat Ribbon Cable (quantity 1) for BCPM, length = 1.2 m
CBL017 Flat Ribbon Cable (quantity 1) for BCPM, length = 1.5 m
CBL018 Flat Ribbon Cable (quantity 1) for BCPM, length = 1.8 m
CBL020 Flat Ribbon Cable (quantity 1) for BCPM, length = 3.0 m
CBL021 Flat Ribbon Cable (quantity 1) for BCPM, length = 6.1 m
CBL022 Round Ribbon Cable (quantity 1) for BCPM, length = 1.2 m
CBL024 Round Ribbon Cable (quantity 1) for BCPM, length = 6.1 m

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.