Browse FAQs

Com’X 510 Login with limited access

Published date: 04 June 2020

Issue
Com’X 510 login shows a ‘Limited Access message’ with restricted access message

Product Line
Com’X 510

Environment
Gateway access

Cause
Case 1:

There’s another user with full access logged in. Current user will have limited access.

Case 2:
There are no other users currently logged in but the message still shows up. This could be due to a user being locked in the logged in state.

Resolution
Case 1:
To get full access other user must first log off from the Com'X web portal.


Case 2:
Manually log out all sessions. In order to do this follow these steps:
  1. In a new browsing window go to <Com'X ipaddress>/applications/monitoring/index.html
  2. Select the Commands tab
  3. Select Catalog
  4. Select "close_actives_sessions"
  5. Execute the command
This should close all active user sessions. Try to log in again.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.