Browse FAQs

Where can I download the latest Cumulative Update and Security Update for PME 9.0 ?

Published date: 06 May 2020

Issue:
Looking for the latest cumulative update for PME 9.0

Product:
Power Monitoring Expert 9 (PME 9.0)

Environment:
Software Installation Files

Resolution:
The latest Cumulative Update (CU2) for PME 9.0 and associated documentation can be found in the link below:
PME 9.0 CU2
-Please note that it is not necessary to apply CU1 before you install CU2. 

The Latest Security Update (SU1) for PME 9.0 and associated documentation can be found in the link below:
PME 9.0 SU1
-Please note PME9.0 SU1 is only compatible with PME9.0 with CU2
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.