Browse FAQs

What is the contact arrangement in a XB2BN411 and XB2BN111 3-Position Maintained Push-Pull Push Button?

Published date: 08 October 2019

Issue:
How do the contacts operate on the XB2BN411 Red and XB2BN111 White  3-Position Push-Pull Push Button operate?

Product Line:
Push Buttons

Environment:
XB2BN 22mm Pushbutton Operators

Resolution:
The button includes 1 NO 1 NC contacts in center position. When you pull the head, the open contact closes, when you push, the close contact opens.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.