Browse FAQs

How do I download Offline Help in EcoStruxure Machine Expert?

Published date: 17 June 2020

Issue
Instead of using the online version of the EcoStruxure Machine Expert Help documents, how do I download a copy to my harddrive so I can access it without internet?

Product Line
EcoStruxure Machine Expert v1.1
EcoStruxure Machine Expert v1.2

Environment
HTML Help Files

Resolution

In EcoStruxure Machine Expert v1.1 follow these steps:
1) Launch Machine Expert Installer
2) Click on "Modify an Existing Software"
3) Select the already installed software version
4) Click on the "Download Online Help" link on the right side of the screen. This will launch the Schneider Electric Help Manager

5) In the Schneider Electric Help Manager, select the Help sections you want to install by placing a green plus sign [+] in the box to the left of the section.

6) Click Apply to begin the installation

The local help files can be launched in a browser from:
C:\Program Files (x86)\Schneider Electric\EcoStruxure Machine Expert\OnlineHelp\Machine Expert\V1.1\LandingPages\en\index.html


In EcoStruxure Machine Expert v1.2, follow these steps:
1) Launch Machine Expert Installer
2) Click on Modify an Existing Software
3) Select the currently installed software version next to "Version:"
4) Select the "Customize version" radio button

5) Click Next
6) Click on the "Help" Tab at the top ribbon

7) Click on Open help management tool. The Help Manager will appear .
8) In the Schneider Electric Help Manager, select the Help sections you want to install (same as in v1.1 above) by marking a green plus [+] symbol to the left of the listed section.
9) Click Apply

The local help files can be launched in a browser from:
C:\Program Files (x86)\Schneider Electric\EcoStruxure Machine Expert\OnlineHelp\Machine Expert\V1.2\LandingPages\en\index.html

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.