Browse FAQs

Does the HMIGTO have passthrough functionality to download/upload to an M340 PLC?

Published date: 19 June 2020

Issue:
Looking for an HMI that has the ability to upload/download an application to an M340 PLC.

Product Line:
Magelis, Harmony, HMIGTO, x80 PLC

Resolution:
The Magelis and Harmony line of HMIs do not have a passthrough function to upload or download an application to an M340 PLC. This function is reserved for HMIs programmed with SoMachine / EcoStruxure Machine Expert that talk to the M2x1 PLCs.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.