Browse FAQs

Is there a cable for HMISTU855 to Modicon Micro (110CPUxxxxx)?

Published date: 29 June 2020

Issue
Replacing an older Magelis with an HMISTU but will not be upgrading the Modicon Micro.

Product line
HMISTUxxx, 110CPUxxxxx

Resolution
For the RS232 RJ45 serial connection the XBT ZG939 + XBT XBT Z9711 combination can be used.

The will work for the Unity Quantum RJ45 RS232 and Modicon Momentum as well.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.