Browse FAQs

What is the part number for a 3 position selector switch rated NEMA 7 & 9?

Published date: 24 June 2020

Issue:
Does Square D offer a Momentary or maintained 3 Position Selector switch that's in an explosion proof enclosure?

Product Line:
Push Buttons and Operator Interface

Environment:
22mm XB4/XB5 Switches

Resolution:
Square D has no product offering available for this application.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.