Browse FAQs

Do we have a handle tie for two FA or KA 3 pole breakers?

Published date: 19 May 2020

Issue:
Do we have a handle tie for two FA or KA 3 pole breakers?

Product Line:
Legacy FA/FH/KA/KH/FI/KI molded case circuit breakers

Environment:
This is for 3P breakers or 2P in 3P cases such as KA/KH/FI/KI 2P which only come in a 3P case

Cause:
Two breakers can be turned ON or OFF at the same time with only one handle throw when a handle tie is used.

Resolution:
Yes. Use FKHT for:
(2) 3P FA/FH or
(2) 2 or 3P KA/KH or
(2) 2 or 3P FI or
(2) 2 or 3P KI or
(1) 2 or 3P FI + (1) 2 or 3P KI

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.