Browse FAQs

Can an accessory be added to an FA or FAL circuit breaker that allows locking ON or OFF?

Published date: 27 May 2020

Issue:
There is a need for an accessory that will allow an FA or FAL circuit breaker to be padlocked in either the ON or OFF position.

Product Line:
Circuit Breakers

Environment:
Applies to FA or FAL series 2 circuit breakers (series 2 breaker have screw holes to allow installation of the accessory).

Cause:
To allow lock-out/tag-out, there is a need to add a device to an existing FA or FAL circuit breaker.

Resolution:
Accessory catalog number HPAFK can be field installed on an existing FA or FAL circuit breaker. This accessory allows the breaker to be locked in either the ON or OFF position.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.