Browse FAQs

Do you need GFR - ground fault relay - with a circuit breaker on the Altistart ATS46 and do you need separate thermal overloads?

Published date: 15 June 2020

Issue:
Ground fualt relay with a circuit breaker, and thermal overloads necesity on the Altistart ATS46 

Product Line:
 ATS46 soft starts

Environment:
 Ground fault relay

Cause:
 n/a

Resolution:
Yes, because fuses are not there to protect from ground faults. Starter has a solid state overload relay.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.