Browse FAQs

What are the repair parts for a HU364A Series E1 Heavy Duty Safety Switch?

Published date: 15 May 2020

Issue:
Need repair parts list for HU364A, series E1

Product Line:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 40560-273-50 (arc suppressor is included) (OBSOLETE WITHOUT REPLACEMENT)
Arc suppressor assembly - 40512-706-50
Lug Assembly - CL20F (incl. 6 lugs)
Line base phase insulator - 40520-253-01
Cross bar insulator - 40511-361-01 (OBSOLETE WITHOUT REPLACEMENT)
Dust shield - 40511-362-01
Mechanism insulator - 40511-371-01 (OBSOLETE WITHOUT REPLACEMENT)
Line base mounting screws - 40205-065-01
Handle knob kit - 4028344050K ( Series E Switches only)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.