Browse FAQs

Can you replace the ST206D, ST306S, ST306ST or ST316ST trip units for CM circuit breakers?

Published date: 14 May 2020

Issue:  
Are the trip units ST 206D, ST 306S, ST 306ST or ST 316ST for the CM-HE or CM-HH molded case circuit breakers still available?  

Product line:  
Molded case circuit breakers

Environment:  
Trip units for Compact CM 1250-2500A circuit breakers

Cause:  
Can you replace a 55722 part number?  It is the ST206D trip module on a CM1600HE.

Resolution:  
The CM breakers and all related components including the ST206D, ST306S, ST306ST and ST316ST trip units are all obsolete.  Replace with a Powerpact R-frame breaker.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.