Browse FAQs

How do you set up the Altivar 28 drive so the start / stop / speed are controlled by the remote keypad?

Published date: 08 June 2020

Issue:
Altivar 28 start/stop/speed controlled via remote keypad.

Product Line:
Altivar 28

Environment:
All

Cause:
N/A

Resolution:
Go to the I/O ( input / output ) menu and set LCC ( local control) to Yes which no allows acces to LFR ( local frequency) parameter for local speed adjustment.  
To change the reference setting you will need to go to the SET menu and change parameter LFR each time desire to change the speed the drive is commanded to run at..

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.