Browse FAQs

What is the mounting hole size required for a 9001O pilot light?

Published date: 25 June 2020

Issue:
Need to know the mounting diameter of the 9001O pilot lights.

Product Line:
9001OA Pilot Lights

Environment:
XB6 Harmony Push Buttons

Resolution:
0.68" or 17.5mm. These pilot lights are obsolete and were replaced by the XB6 16mm lights. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.