US Electrical Fires 2003-2014*
378 / 1290
$1.4 Billion
Are You Protected Against Electrical Fires?
Learn how our dual function circuit breakers can help
Square D™ Dual Function Circuit Breakers: An Industry First!
Square D™ Homeline™ Load Centers Plug-on Neutral CAFI & Dual Function Circuit Breakers
A Safer Home
Superior electrical safety for homeowners
Electrical problems spark an estimated 25,000 home fires and cause more than $1 billion in residential property damage each year. (US Electrical Fires, 2003-2014*). Electrical wiring, cords, and plugs, switches, receptacles, and outlets can be the source of tremendous damage to your property or worse, your family. Protect yourself with Square D™ circuit breakers.
Just like the airbags in your car and technology on your smartphone, circuit breakers are more advanced and sophisticated than ever before. Square D™ circuit breakers are engineered and designed to help keep you, your family, and your property safe from electrical hazards that were previously undetectable. A circuit breaker “trips” and shuts off power when it detects an issue on a circuit that could possibly cause an electrical fire.
To help you better understand the protection of your home electrical system, let's take a look at a few state-of-the-art types of circuit breakers.
Ground Fault Circuit Interrupters (GFCIs)
GFCIs are designed to protect people from the dangers of electrical shock. These circuit breakers are typically installed on circuits where water sources may be present. The National Electrical Code (NEC) requires ground fault circuit protection in the garage, outdoor areas, bathrooms, and in spa areas within the home.
The QO and Homeline Ground Fault Circuit Breakers provide Class A protection, sensing and responding to very low levels of ground faults by tripping or shutting off power, preventing serious electrical shock to people.
* The Federal Government, the National Fire Protection Association, and US fire departments track the incidence of electrical fires across the United States and categorize those fires based on their causesProduct information for Residential Circuit Breakers
Combination Arc Fault Circuit Interrupters (CAFIs)
CAFIs help provide protection against dangerous arcing; the precursor to many electrical fires. Square D QO™ and Homeline™ CAFIs help protect people and property from fires caused by electrical arcing. These devices continuously monitor the branch circuit and trip when a potentially dangerous condition is detected.
Dual Function (CAFI + GFI) Circuit Breakers
The innovative Square D QO and Homeline Dual Function Circuit Breakers combine two critical, state-of-the-art technologies: Combination Arc Fault and Ground Fault (Class A) Protection in one circuit breaker. Dual Function Circuit Interrupters provide a higher level of protection than any other residential circuit breaker. These devices combine both Ground Fault Protection and Combination Arc Fault Protection in a single device. And these devices protect the entire circuit on which they are installed, not just a part of the circuit like electronic receptacles (GFI or AFI) do.
The U.S. Consumer Product Safety Commission (CPSC) estimates that Combination Arc Fault Interrupters could prevent more than fifty percent of electrical fires that occur every year.