Roll over image to zoom in

9070FB3A
Product availability: Stock - Normally stocked in distribution facility
50/60 Hz rated
Customer installed accessories (Finger-Safe covers, fuse blocks, fuse clips)
Designed with various temperature classes
Factory installed fuse blocks are pre-wired and mounted on top of the transformer,
UL E61239, CSA LR37055 Guide 184-N-90
Environmental Data
Use Better
Packaging made with recycled cardboard
Yes
Use Again
Take-back
No
Need more information? Check our technical FAQs!
Easily find answers to the most frequently asked questions.