Roll over image to zoom in

4 videos
HPAFD
Product availability: Stock - Normally stocked in distribution facility
Used to padlock circuit breakers in the ON or OFF position
Includes one padlock attachment and required hardware
Compatible with PowerPacT E/F circuit breakers
Easy plug on circuit breaker that’s compatible with Square D™ QO Loadcenters
Complies with UL 489 listed, CSA, and IEC standards
Environmental Data
Use Better
Packaging made with recycled cardboard
Yes
Use Again
Take-back
No
Need more information? Check our technical FAQs!
Easily find answers to the most frequently asked questions.