Roll over image to zoom in

KCF1YZ
Product availability: Stock - Normally stocked in distribution facility
Reliable operation with padlockable handle
It is suitable for 2 operation methods: directly on switch body or through a shaft extension
It ensures high protection degree to the mounting
With numerous advantages to meet OEM’s most common needs
Environmental Data
Carbon footprint (kg CO2 eq, Total Life cycle)
30
Use Better
Packaging made with recycled cardboard
Yes
Use Again
Take-back
No
Need more information? Check our technical FAQs!
Easily find answers to the most frequently asked questions.