Simplify Installation and Reduce Inventory
Whether you need the standard pigtail or the time-saving Plug-on Neutral Square D™ QO™ and Homeline™ Dual Function Circuit Breaker, your installation is sure to be efficient. These innovative circuit breakers combine two state-of-the-art technologies — Combination Arc Fault and Ground Fault (class A) protection — into one easy-to-install device. Square D™ Dual Function circuit breakers give contractors a better solution by reducing cost and eliminating the hassle of using two separate devices to provide critical protection.
Quick Plug-on Neutral Connections
QO Plug-on Neutral (PoN) Load Centers interiors are engineered to accept PoN CAFI circuit breakers for a quick Plug-on Neutral connection on every circuit. Designed for reliability, and a time and labor saving installation, the QO Plug-on Neutral Load Center contains an extended neutral bar that directly connects to the QO Plug-on Neutral CAFI circuit breakers.
Easier Than AFCI Receptacles
AFCI receptacles are harder to install than standard receptacles. Every electrician knows how hard it is to squeeze all that wire into the small outlet box. You can also accidentally break the wire feed, causing rework. Simplify your installation by using a Dual Function circuit breaker, and remove the wiring headache by using standard receptacles.
One Centralized Location
You no longer have to hunt for the tripped GFCI outlet when using Dual Function circuit breakers. Everything is at the load center. Just look for the purple test button.