Browse FAQs

How do you determine the manufacturing date for the ATV61 / ATV71 drives?

Published date: 18 May 2020

Issue:
Determining the manufacturing date for the ATV61/ATV71.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Warranty requirement.

Resolution:
Get the serial number from the bar code sticker mounted on the drive housing or in the (Drive menu) Identification menu 1.11. The manufacturing date can be obtained from the serial number in terms of manufacture's year and week of the year the drive was built.
Example: serial number reads  8B13090000 manufacture's date reads
8B= manufacturing location
13 = year
09=  week

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.