Browse FAQs

Why isn't the Ready LED on when power is applied to the 170ANR12090 module ?

Published date: 18 August 2020

In addition to having power connected to this module, you also need to have a non-zero value in the System Information register. This register is the first output word register which is IO mapped or Traffic copped. Valid settings for this register are 0001 - FFFF hex. If a non-zero value is added to this register and the ready LED is still not on, then there is a hardware problem with the module.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.