Browse FAQs

How do I configure the I/O scanner for a Quantum NOE771xx so that Advantys STB I/O does not intermittently drop out?

Published date: 24 April 2020

Goals and Symptoms

How do I configure the I/O scanner for a Quantum NOE77100 so that Advantys I/O does not intermittently drop out?

Facts and Changes

Using Advantys Ethernet I/O (STBNIP2212) with a Quantum NOE771xx and Quantum CPU programmed in ProWorxNXT. I/O scanner is configured for 1500ms health timeout, 0ms rep rate, zero fallback, and usually less than 10 read and write count. On the Advantys, the inputs (like pushbuttons) are dropping out for a scan every 1-2 seconds. What is the proper configuration to eliminate this and give me steady inputs?

Causes and Fixes

Change the Repetion rate setting of your IO scanner to 20ms.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.