Browse FAQs

Can the scale factor be manually changed on the Series 200, 700 Power Meter to display more resolution on the display?

Published date: 20 May 2020

The Series 200, 700 Power meters do not have a command interface that allows the user to change the scale factors. The scale factors are automatically determined based on the CT and PT ratios. If manually setting the scale factors is required then consider using the Series 800 Power Meter.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.