Browse FAQs

What is the minimum and maximum rated voltage on which the Vigi C120 can operate.

Published date: 05 September 2020

The minimum/maximum rated voltage on which Vigi C120 range can operate is as follows:
 
  1. For VigiC120 30mA - Minimum Voltage 196V / Maximum Voltage 456V
  2. For VigiC120 300mA - Minimum Voltage 189V / Maximum Voltage 456V
  3. For VigiC120 500mA - Minimum Voltage 175V / Maximum Voltage 456V
     

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.