{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
You are currently viewing the content available in Vietnam. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What type of fiber optic cable is recommended for the M340 or M580 BMXNRP0200 fiber optic repeater?

Issue
BMXNRP0200 fiber optic cable specification

Product Line
M580, M340, BMXNRP0200

Environment
Unity Pro, Control Expert

Resolution
Below are the parameters specified for the Fiber Optic cable:
  • the wavelength of the optical signal: 1310 nm
  • the cable index: use graded-index cable only
  • Fiber size - 50/125 μm or 62.5/125 μm or  9/125 μm
For most multimode optical cable links, the use of 62.5/125 μm cable is recommended because of its relatively low loss and signal distortion. Select the fiber optic cable that meets the demands of your application. Multi-conductor cables are recommended. Most 62.5/125 μm cables are rated at 1.5 dB loss per km. With a multi-conductor cable, pairs come with an attenuation specification as measured, which is less than 3.5 dB/km.
The fiber ports, in both multi-mode and single-mode modules, use LC-type connectors.

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.