Browse FAQs

What can caused an "HTTP Server failed to run on specified port" error when using the Vijeo Design'Air app?

Published date: 19 August 2020

Vijeo Design'Air uses internal port 6002.  Vijeo Designer V6.2 does not allow you to change that port.

The external port can be setup to 6002 or something else if you have more than one HMI in the router port forwarding configuration but the internal port is always 6002.

The Webserver port is usually 80 and should not be changed to 6002 otherwise you will have a port conflict error.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.