Browse FAQs

What does the designation NC or N/C mean on an IO module's wiring diagram?

Published date: 10 May 2018

 NC or N/C designates no connection. This pin is not integral to the modules operation and need not be connected.
The NC or N./C terminals are normally isolated from the module's circuitry. 


*Note: The 800 series family of  I/O is obsolete. Please consider alternatives offered in the Quantum or BMX families of IO .


R-3122018

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.