Browse FAQs

How to gear in two LXM28 drives in SoMachine?

Published date: 10 September 2020

Issue:
Setup function block GearIn_LXM28 so that the client and server drives follow each other perfectly

Product Line:
LXM28

Resolution:
The NUM of the GearIn_LXM28 function block should be set to 1280000 and the DENUM should be set to 8192 (2048 x 4).
This will make the perfect gear between the client and server.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.